Loading
Case Study | Digital Transformation Thought Leadership
Recent ActivityRecent Activity

Cytiva Brings Digital to Life in Life Sciences

Better use of digital technologies and automation helps biomanufacturing companies realize economies of scale with flexibility, efficiency and confidence.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Female lab technician writing information on a test tube with a marker after viewing results in a microscope

Cytiva customers undertake life-saving activities ranging from fundamental biological research to developing innovative vaccines, biologic drugs, and novel cell and gene therapies.

Cytiva’s job is to supply the tools and services they need to work better, faster and safer, leading to better patient outcomes. More than 7,000 associates across 40 sites support the company’s vision of improving access to life-changing therapies that transform human health.

As part of its digital transformation and Industry 4.0 initiative, Cytiva wanted to create a connected digital enterprise to help improve internal operations and decrease time-to-market for end customers.

Chevron DownChevron Down

Enabling the helpers

Enormous amounts of time and money go into developing new pharmaceutical and medical products, and there’s a small window before each new product’s patent expires. Reducing time from inception to market is enormous because it allows the product to capture market share longer.

“Now more than ever as an industry, we must get smaller, faster and more cost-effective in the way we manufacture drugs, vaccines and therapeutics,” said Kevin Seaver, executive general manager, automation and digital at Cytiva. “By automating processes and analyzing data, we can rethink every step of drug manufacturing and realize economies of scale with flexibility, efficiency and confidence.”

Streamlining the deployment of systems, reducing islands of automation, and decreasing the time spent on gathering and cleaning data all can help biomanufacturing players accelerate their time to market.

“Our aim is to help companies go from seven years down to three or four by doing much of the engineering and automation work upfront,” Seaver said.

Integration and automation across the value chain

The Cytiva Figurate automation platform includes control and communication capabilities that turn data insights into productive outcomes for both upstream and downstream process efficiency gains.

To develop and put its Figurate platform in place, Cytiva adopted the Rockwell Automation PlantPAx® system and used its own Unicorn software to automate its bioprocess equipment. Data is made available through MES applications and can be integrated to include electronic batch records, scheduling and more.

The platform is designed to dramatically streamline deployment of systems for end customers. There are options for Rockwell Automation systems and others, depending on the end-user’s specific needs. Standardized digital libraries – such as product code that's been tested, documented and validated – also can create more efficient process development all the way through manufacturing and automation.

For example, a customer using our PlantPAx system can operate it as a single standalone system but also operate it together with other systems. Through integration the customer can transfer not only the biopharma material but the data along with it.  

“A few years ago, automation was a boat anchor. Now, we are one of the main differentiators in the company.”

Leveraging the power of analytics and data

Within The Connected Enterprise®, customers have all the documentation they need electronically and can release it to manufacturing immediately. Additionally, Figurate can bring process data up to the cloud where it can be combined with additional operational data. Using advanced analytics, these valuable insights can be used to improve operations and can then be fed back down to the system to optimize processes.

“There’s cost, time and quality. Usually if you want to gain on any one of those three you have to give up something,” Seaver said. “But we can be faster. We can deliver it more cost-effectively since we’ve already done all that upfront work. And quality is higher, too, because we’ve validated the code as well.”

Cytiva’s automation lab and a room called The Sandbox house servers with different types of applications that are being developed and tested. This testing environment allows Cytiva to prove everything out before it goes to customers. If customers have questions or problems they can bring them in and test them, creating a collaborative environment.

Delivering pre-tested solutions

Cytiva's FlexFactory lines, featuring Figurate, include media and buffer preparation, cell culture production, harvesting, purification, viral clearance, sterile filtration and bulk formulation processes. All of these can be combined in modular KUBio clean-room shipping containers and delivered to biomanufacturing customers, essentially ready-to-go.

"Our KUBio systems are effectively shipping container-based production units that allow us to build an entire factory in less than 18 months," said Seaver.

Additional benefits beyond speeding up time-to-market include 10-20 percent increases in production throughput, availability and production employee efficiency, as well as 5-30 percent decreases in energy use, scrap material, batch release time, maintenance and downtime investigations.

Published December 2, 2020

Topics: Digital Transformation Life Sciences FactoryTalk InnovationSuite
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Digital Thread
Digital construction of a plant
Capability
Digital Thread

What is Digital Thread? Rockwell Automation can connect critical business functions and accelerate digital transformation with a unified enterprise approach.

Explore Our Capabilities
MES Solutions for the Life Sciences Industry
Equipment connected with two medical employees sitting viewing results
Brochure
MES Solutions for the Life Sciences Industry

PharmaSuite MES provides production operations management to help you meet regulatory compliance, achieve operation excellence, increase supply chain effectiveness, and meet your goals.

Download Now
Pfizer: Changing Lives with Digital Transformation
Client reviewing label directions on medication
Case Study
Pfizer: Changing Lives with Digital Transformation

At Pfizer, a multi-year digital transformation is driving improvements in cycle time, yield, and right-first-time quality.

Read Now
The Facility of the Future eBook
Lab technician placing test tubes in a holder
Brochure
The Facility of the Future eBook

Does your facility operate at its full potential? Download the eBook to learn how to deploy smart, fast, and flexible Life Sciences facilities.

Download Now
  • Contact Sales
  • Contact Customer Care
  • Contact Technical Support
  • Phone Support
  • General Questions
  1. Chevron LeftChevron Left United States Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Case Studies Chevron RightChevron Right
Please update your cookie preferences to continue.
This feature requires cookies to enhance your experience. Please update your preferences to allow for these cookies:
  • Social Media Cookies
  • Functional Cookies
  • Performance Cookies
  • Marketing Cookies
  • All Cookies
You can update your preferences at any time. For more information please see our {0} Privacy Policy
CloseClose